What Windows versions can 800xA ver 6.0.2 be installed on?
According to manual 3BUA000500_T_en_System_800xA_Third_Party_Softwar..., Win Server 2012 R2 is required from 800xA ver 6.0 for servers.
Is that true if I want to install a Standalone-system?
Is it worth a try, to install on a Win7 Enterprise (64bit)? Anyone tried that?
Thanx
/Martin
Answers
From the version 6 release notes:
800xA 6.0 requires Microsoft Windows 8.1 and Windows Server 2012R2.
800xA 6.0 can be used together with Microsoft Office 2013.
Visual Basic Process Graphics (VBPG) is not supported in System 800xA 6.0.
VBPG based graphics needs to be replaced by Process Graphics 2 displays
before moving applications to 800xA 6.0
Some functions require server software
Winows 8.1
Add new comment