2 Q:1. pls. send me the complete (ProjectTree.prt) of waterplant. 2. How to insert devices (FGR) in Graphic editor
For Q1, my ProjectTree.prt is not complete, appreciate to send me the full .prt file at my e-mail khalid2757@hotmail.com
Regarding Q2, I am trying to draw few pumps, FCV and other instruments to Graphic Display, but I cound't find these devices. appreciate your help as well.
Thank you,
Khalid,
Answers
Hello!
I guess you are talking about the Water plant from the Freelance Quick-Start CD. You can order your CD free of charge at the link below.
Additionally I attach the project files from the CD here.
Unzip the 2 CSV files into the Export directory of the Freelance installation and import them into the Control Builder F.
Please make sure to use at least Freelance 2013 or higher to be able to import the projects. A compatible Freelance Demo version is part of the Quick-Start CD.
Hope that helps
P.S. The graphics for pumps and other devices for FGRs are part of the Macro Library that comes with the Freelance Installation.
Add new comment