How to enable force access in faceplate of sil3 application.I could not force through faceplate any changes need.
Answers
you have to provide confirm and access enable in control module in each level ... starting from aplication, single controle module, til the level where the signal faceplate is... the control module in Engg workplace has a SIL tab and in that the name of the say MABlock for example, there it will say option for confirm and access enable. then the Di in the SIS SM811 module should be set. Then the application in CBM has a property to set number of forces allowed per application. then wehn you download you should be able to force signals.
Add new comment