I have created one function block in library ,but I could not use tat in sil3 application
Incompatible sil level on function block error is coming
Answers
Hello.
You can do a right click on the Function block in the library, choose Properties/Safety Level/SIL 3.
Tung Dao.
Go in Properties and change your SIL level.
Also, make sure you change level of FB,and then attach SIL library to Application as SIL.
Plus do the same in HHarsware Tab also
Add new comment