Download problem to a redundant Advant Controller 160
I have a problem when I try to download the program to an AC160 in redundant configuration.
When I download the program to the CPU appear a message like this:
"The redundant CPU must be in tool mode".
I`ve never seen this message before.
I´ve tried to download both CPUs in STOP mode, but only I can download the first CPU, if I try to update the second CPU with the command in Advabuild, an error occurs.
Answers
This question has not yet been answered.
Add new comment