Parameter Index of MNS iS to establish acyclic communication
PROFINET CI871 established the MNS iS communication using MLink and able to operate MNS iS. We need to establish PRONINET acyclic data communication with MNS iS using Read/Write data on command via IEC 61131-3 application (AC800M controller used).
Where do I get the Parameter Index of MNS iS to establish acyclic communication?
What is the API for MNSiS?
Answers
This question has not yet been answered.
Add new comment