How to configure the Control Builder Plus application for the PM573-ETH PLC through a router
We have installed a PM573-ETH PLC at a remote site with its default address (192.168.0.10). Our It guy give us a specific IP address to reach this PLC, he has to root his specific IP address to the PLC address. Where do I configure this specific address in the Control Builder to communicate remotely with the PLC.
Thank you for your help.
Voted best answer
Hi
I'm not sure to have correct understand your question, you need to read as "web server" the remote cpu? Or do you need to modify of the program?
In the first this case, you must define the remote access via remote VPN of the cpu adress, but you need assign the adress in the program with IP config tool, in this mode you can read the web server page that you have wrote during programming.
Hope this help you
Add new comment