800xA 6.0.2 Installation problem
Prepared a windows 8.1 according to prereqs etc.
(Exactly as two other PC's which did not experience the same problem)
Running Setup.exe in install medium, entered user names, pwd's etc. resulted in error.
It mentioned something about "Open System Installer Notification Icon menu and select View logs." (see attached screenshot).
I did not find any icon nor any log files and I have no idea why it failed on this machine only.
Then I restored the machine to an earlier restore point and tried again, this time the setup shows progression bar for just about a minute or so and simply dies without any seemingly tracks of anything.
What do I do wrong and what can I do to proceed ?
Voted best answer
As per attachment first Enable the view log option from right click on System 800Xa Installer agent Icon or directly you can see the log from below path-
C:\ProgramData\ABB\800xA\SystemInstaller\Agent\ActivityLogs
Hope it will help you.
Answers
Perhaps this error (I see it often):
Add new comment