ABB OS520 (Unix base) Hard disk damage and procedure to install the software.
In 156 MW Gas Turbine at Hazira,Gujarat....
ABB Advant control system and Operating system used OS 520(APC OS 2.3/1)
ABB System installed year 2000.
There is three Operating Station and One operating station Hard disk damage and OS not working properly.
Question : How to rectify the Opearating station problem and Procedure to install the software.sequence of install the software and any support.
Voted best answer
The installation is described in the release notes for Advant Station 500 OS.
Installation start at chapter 4.
- Replace hard disk (ABB Logistic Center has disk as spare part)
- Get media tape or CD
- Boot on media
- Select options (Graphics Builder, Online Builder, etc)
- Get APC media
- Install APC option (follow separate release note)
- Restore displays from backup or via Display Transfer from other OS
- Voila!
Add new comment