What methods exist to obtain backup micro sd memory PM AC 900F ABB
Tengo un DCS con los controladores AC900F, en configuración redundante Para hacer una copia de seguridad en la memoria micro SD, sólo se puede hacer con las opciones que el menú de pantalla dispone? sólo puede ser descargado desde el controlador de la memoria micro SD de la pantalla? Desde el "Control Builder F" Puedo hacer una estafa a la micro SD, si no tengo la pantalla? gracias por tu ayuda
ENGLISH Version text
I have a DCS with AC900F controllers, in redundant configuration To make a backup in the micro SD memory, can only be done with the options that the screen menu has? Can only be downloaded from the micro SD memory controller of the screen? From the "Control Builder F" I can do a scam to the micro SD, if I do not have the screen?
thanks for your help
ENGLISH Version text
I have a DCS with AC900F controllers, in redundant configuration To make a backup in the micro SD memory, can only be done with the options that the screen menu has? Can only be downloaded from the micro SD memory controller of the screen? From the "Control Builder F" I can do a scam to the micro SD, if I do not have the screen?
thanks for your help
Voted best answer
Hello,
Yes, Right user can take backup on SD card from display only, can not be possible from CBF/Freelance Engineering. So you need display. Go for one.
you can use some other features and controller configuration is easy using display.
Hope that helps.
Add new comment