800xA 6.0 System restore with node renaming
Hi Folks,
What is the proper way to make a system restore in version 6.0 when I also need to rename the nodes during the restore?
I have tried to following the manual 3BSE046784-600 page 99-100, where the Configuration Wizard is used.
1. During restore I also changed the node names (as on page 127).
2. When I connect the node again I use the configuration Wizard as stated on page 100 - Is that the right way? (When the wizard is started a waning tells me that System configuration console should from version 6.0 be use to connection client node)
I end up with me a fully working system (Where alle nodes has be renamed), but inconsistent system configuration console with still the old names and connection problems!
Any suggestions?
Answers
Hi,
From SV 6.0 onwards, System Configuration Console is recommended for create a new system,restore system etc. The machines with new names can be added to the system using System configuration console.
Hi
It turns out that this is not possible via SCC in 6.0.1, 6.0.2 and even limited in 6.0.3!
A workaround would be to overwrite the two systen installer aspects: Admin Structure/Domains/YourDomain/System consiguration & System Configuration State aspects with a exported aspect from a clean new system with the new names.
Add new comment