IEC 60870-5-104 protocol with EI 813F / EI 803F
Hello,
I need help for this issue. I have a AC 800F-Controller with software version Freelance 2013 SP1 RU2. I want to use the EI 813F communication module for using the IEC 60870-5-104 protocol. The communication does not work, I only get the state "10". If I use the EI 803F communication module the communication works! Is there a difference between the EI 813F and EI 803F communication module for using the IEC 60870-5-104 protocol? I have another AC 800F-Controller with the same configuration and there the communication works with the EI 813F module. Anyone knows this problem?
Answers
Hello,
There is no known problem related to such a description.
It currently seems to be a single case with a specific hardware issue.
Therefore, try to isolate the problem :
# if you confirm that you can use the EI813F module in another controllers
it could be a hardware issue for the first controller ???
To receive a detailled explanation for this situation, I suggest you to contact your ABB supportline.
Add new comment