Any manual way to start 6.0.2 update of a node?
On a running 6.0.2 system with Base RU3 when moving a client from a 6.0 to a 6.0.2 system, it seems that I cannot do a deploy and upgrade through the SCC.
After running the 6.0.2 NPT on the client, is there any way to start update of the client manually?
Same problem with the Base RU3, how to start manual update?
This question also seem to be an issue when preparing a new client or server, installing 6.0.2 on a new machine, it still need the Base RU3 update before it is possible to add the machine to SCC on the primary aspect server.
Answers
This question has not yet been answered.
Add new comment