structural backup of 800xA 5.1 into 800xA 6.0.1/6.0.2
Hello All,
I have one doubt regarding this & the problem is I have one system with 800xA 6.0.1 working in live condition so I cant do anything new on the system which could effect it.
My doubt is can we import the structural backup created in 800xA version 5.1 Rev.D into the systemworking on 800xA version 6.0.1 without effecting its working..?
can some one please clear my doubt.
Answers
For using 5.1 RevD backup,first take a maintenance backup from 5.1 RevD and create a single node of 6.0.1/6.0.2 with same product and restore the 5.1 RevD Backup in single node, then you can Export and import AFW backup easily as per your requirement.
Hope It will help you.
Hi!
Whats the issue?
You have to perform an upgrade (incl restore backup) from 5.1RevD to ver 6. For this you'll need a standalone system (primary aspect server) according to your conditions. I would perform the upgrade and then use Import/export tool to move specific parts to your new system.
Concerning Basic History Data it's possible to just copy and paste.
Check the upgrade manual: 2PAA111694-600_E_en_System_800xA_5.1_to_6.0_Upgrade
Good Luck!
BR
The answer vary from "Oh yes!" to "No!" dependung on what your "structural backup" consists of...
- Alarm List, Process Graphics (PG2)... yes!
- 800xA for Advant Master... oh yes...
- Control Builder M... mmm probably no...
- etc
Add new comment