Variable list export and import with OPC addresses
Hello,
In freelance, Is there a way to export and import variable list with OPC addresses.
Answers
Hello asad1837,
Yes, there is. Simply go to Variable List, choose Edit menu and Export.
Choose a directory, name and type for the export file and then You can choose what information You want to export in a window like this:
Choose OPC Address (and any other options You find useful) and click Export button.
Viola! Variable List with OPC addresses exported.
Hope this helps,
Mike
Hello MMM,
Thanks for your precious time. Refer to the question above i am attaching pics that are steps i am following.The dialoge box in step3 file is not showing any other type except .eam type. Even if i am saving this file as .csv, same format is saving and no dialoge box is appearing for selecting OPC, as you have mention before.
/asad1837
Hello asad1837,
Now I understand the problem. You are using old Freelance version. It's most probably v8 or v9, but the function I mentioned is avaliable since v2013. I didn't ask for Your softs version, becouse You mentioned Freelance Engineering, a name which is used from v2016, so I jumped into conclusion that You are using the newest one...
The only thing You can do in older Freelances is to export whole project and extract OPC addresses from project export .csv file. Search for [BEGIN_OPCADDRESSSECTION] tag. There You will find variables with OPC addresses (but only those, so if You need all variables, You would need to merge info from this part of file with info from [BEGIN_EAMSECTION] part).
Hope this helps,
Mike
Add new comment