How to open CBF, if Password forgetted?
Software:- Freelance-9.2 SP2
One of our client has forget password for opening CBF.
Is it possible to derive the password from C drive.
Answers
If it is the Projekt Password, there is no easy way to find it out.
Might be abb suport can help you.
But i think if you have a csv-file of your project, you can remove the part with the password and import this file (I thik it works in Version 9.2). But then you have to do a load hole station.
Also the csv-file should be a current version of the project or you know the changes in the software.
Hope that helps.
Help if the CBF password has been lost :
For Freelance Users , there is no methode to reset or to bypass a CBF password.
In such a situation, either the user have an old project where no password for CBF was configured or Freelance R&D can try to reset CBF the password.
For the second issue (reset of CBF password), Freelance R&D can developp a tool to try first to open the Project and then to reset the CBF password. The freelance version determines the needed effort. If this solution is choosen, please contact the ABB Supportline for Freelance, the needed effort will be charged to the purchaser (customer or project manager)
by JuergenV Rank: 70 on 11/7/2016 1:23:06 AM | Like (0) | Report
Project password or Security lock passwords?
Add new comment