'#NAME?'Appearing in reports?
Software: 800XA-5.0 SP-2 PLC Connect
Redundant Server, Reports are configured in Primary Server.
As per schedule reports are generating but instead of real values '#NAME?' are appearing in excel reports. Rest everthing is working fine, OPC data and alarms are healthy.
Tried re-configuring tempelate also but still same problem persist.
Error:- While opening excel file following error popup is appearing:-
'Microsoft Office Excel can not find 'ABBDynTime' on 'ABBDataDirect.xla'
Answers
Have you upgraded Excel or installed some Microsoft hotfixes lately?
Try reinstalling the ABB DataDirect software kit; try the latest version unless you already have it.
The most recent DataDirect version have the following build ID: 5.0.7911.0926 and is bundled with 5.0 SP2 RevE media.
Add new comment