Access level password on Digivis
Hello !
I want to know if it's possible to have different access password in Digivis. For example, if I want to change a set point, only level 1 operators can change it. For another action, it's only level 2 operators, etc..
For the moment I can only have a password to leave Digivis.
Thanks a lot !
Eric
Voted best answer
Yes of course, it is possible.
For this you mast have security Look.
It's an additional feature.
But if you use it, the rights are only given to the whole object.
That means if an operator has the right to operate, he can operate everything of the object or nothing.
It's only possible to decide to have the rights no permission, observe or operate the object.
For example it is not possibel to give only the right to acknowledge but not changing the setpoint.
Answers
Okay, I have to use Security Lock. I don't have the license, so I understand why I can't have password for operators.
Thank you !
Eric
Add new comment