License error while loading license as extension
Hi,
I have an 800xA system with smart client configured.Previousuly I havd only 2 users of smart client. Now I have 4 users. So I decided to add 2 more smart client license.
Got the new license file and tried to load the file as extension.I have the same system ID (SID number) in 800xA license and smart client license.
I got an error saying "Microsoft .Net Framework"...Input string was not in a correct format ...Please refer to the attached screen shot.
Let me know anybody face the same problem. How I can fix the same.
Any suggestions are welcome.
Answers
Corrupt .SLA file?
Also, I'm not sure Load Extension is the correct procedure. I seem to recollect "extend" to be used when adding a temporary extension, eg a few more Control Builder M licenses on top of the permanent license, eg during engineering phase.
Try loading the same file in another CLS - if it popup the same error, the file is likely not OK. Speak with your sales representative about a replacement file.
Add new comment