Information Manager and 800xA History
What principal difference between 800xA History Signals-Logs and History Logs (for example catalog number 3BSE079539R1 and 3BSE078843R1) Is it possible to coexist 800xA History and Information manager in one system? Do I need both or their function duplicates?
Voted best answer
Absolutely, both IM and 800xA History can exist in the same 800xA system. Obviously this requires licenses for both, which can be expensive for the customer. When configuring History Logs for signals, you should use independent Log Configuration aspects for their configuration to prevent any mix up. As for the current capabilities, only the IM is utilized to administer the PDL information for Batch. This will be integrated into 800xAHistory in a future release. There are other considerations to make if deciding to utilize either the IM or 800xAHistory but not both, however, the local sales representative can address this if necessary.
Regards,
Geof Ledin
US-OCS-SL-L3
Add new comment