AC80 and NPBA-82 for ProfiBus communication to external Siemens S7 CPU
Dear All,
On our project we want to extend an existing AC80 controller on a RTG crane with a NBPA-82 ProfiBus DP module for communication with a foreign PLC system. The module itself has been organized including FO cables, so from hardware point of view everything is prepared.
Our issue is the integration into the PLC program. We are using the following versions:
- Function Chart Builder Release 6.2/1
- Node type: AC 80 1.1, Base SW: AC 80 BASE SW* 1.1, Additional options: OPT: Emb. Modbus I 1.0
In the manual "en_NPBA82InstStartupG_a.pdf" a type circuit PROF5EXC is described, which cannot be found on the enginering system. As well the exact integration into the system is not clear.
A programming example of an AC80 controller w/ NPBA-82 module as well as the type circuit PROF5EXC for FCB 6.2/1 would be very highly appreciated.
Thank you in advance for your support!
Best Regards,
Norman Kraushaar
Answers
This question has not yet been answered.
Add new comment