How many number of MB300 Nodes can be configured under CI855 module..
How many number of MB300 Nodes can be configured under CI855 module..
Limitation and documentaion/manual referneces stating the same.
Answers
Same answer as in previous thread.
A CI855 plays by the same MB300 ruleset as the Advant Controllers do.
Do also check the Control Builder M On-Line Help for CI855.
Add new comment