Problem 800xa 5.1 Rev. A, adress in the driver modbus for PLC connect
after upgrade my system at the 5.1 Rev A version a new feature in the PLC connect is available for the TCP Modbus driver , the bit address in a word for boolean signals, (in the manual view the reference for adress example HRAxxxx,y when "y" its a bit 0 - 15 abd xxxx its a 4xxxx modbus register.
mi problem is "the new feature not work "
mi problem is "the new feature not work "
Answers
Requested to contact with local ABB L3 support line. as per RN 800xa 5.1 Rev. A/B seems it is fixed issue.
Add new comment