AI531 8 Channel Analog Input, Does the card maintain analog circuit integrity when the PLC loses power
Answers
Hi
could you explain what you real mean or need? The modules of AI 531 are supplied with a process voltage of 24 V DC, you can use one different 24 V DC from battery surge or UPS, but it's no clear what you mean for "integrity"
If you give us more information, we can help you better
When the PLC Loses power, the configuration is retained(including the parameter settings, range selections, scaling etc).
Signal Integrity: Do you mean loop integrity,as in a PID Loop? Please clarify
Add new comment