PLC on 800xA via Ethernet IP
A potential customer has asked this question regarding PLC connectivity to 800xA:
Has ABB done any migration with the SLC EtherNet/IP scanner (1747-AENTR)? This puts the SLC PLC on Ethernet. I would like to know if we there is a solution where a redundant CI873 could communicate on the same network, or will we need to put ControlLogix in between as a de-facto Pyramid Integrator.
Answers
RSLinx is an excellent OPC server. If it talks directly to your Allen Bradley SLC, then it will work very well with PLC connect.
Add new comment