Graphical representation of the variables Connected in Hardware.
Hi,
I want to graphically represent the variables Connecetd in Hardware. Is there any way? I am using 800xa rev C FP4
Answers
Hello,
In above example instead of "S01CM_LT1:In.Value", select the variable which is connected in the hardware.
PG2 can only present data from OPC.
AFAIK, the name of bound variable is not exposed over OPC.
Add new comment