0x4ABF0: Unable to contact CLS server the client has been granted temporary license
Hi,
I am getting license pop up message in OWS/EWS,this occurs only when I open Operator workplace.
"0x4ABF0: Unable to contact CLS server the client has been granted temporary license"
Operator_WPL is within the limits. Didnot cross the max allowed limits.
800xA 5.0 SP2.
Thanks
Answers
I remember a similar issue on 800xA 4.1. It was gone after re-entering the name of the license server in license status viewer.
- Open "License Status Viewer"
- Tools --> Change CLS Machine
- Enter the name in "New CLS Machine" (same as in Current CLS Machine)
- Apply
- Reboot
As per the error messgae, System is unable to contact CLS Server. You have to chage the CLS Server to correct one and then reboot.
Add new comment