CHMI800 SPOL library - Alarm acknowledge of object error
Hi
I'm using MotorUni in the CHMI800 SPOL library and a MotorUni function block in the PLC. It seems to work fine except for resetting object alarms.
If I have an "objErr" on the motor object in the PLC (due to feedback timeout when starting) I cannot reset that alarm by clicking the red triangle in the SPOL MotorUni faceplate.
It seems that the tag "2_ObjErrAck" connected to "InteractionPar.objErrAck" never goes true in the PLC when the triangle is clicked. The OPC tag has Good quality.
Shouldn't the "2_ObjErrAck" tag be activated when clicking the red triangle in the faceplate?
Right now I have to reset the object error by using the "AlarmReset" input on the MotorUni function block in the PLC.
Thanks in advance!
Answers
This question has not yet been answered.
Add new comment