Plase help me to establish a communication betweern Siemens VFD on profibus DP and ABB conteollers - AC450 , AC410
1st system
Communication siemens VFD on profibus DP and ABB AC 450 Controller.
2nd system
COmmunication siemens VFD on profibus DP and ABB AC 410 Controller.
Thanks & Regards
ABHIJITH
Answers
Honestly ....
Dont.
http://www402.abbext.com/how-connect-...
Otherwise,
You will need a CI541 profibus submodule and an available SC510 slot to install it into. To configure it, Read The Manual
Copied answer here from duplicate thread, avoid posting duplicate question many time.
Thanks for your understanding.
"Hi!
With the Advant controllers, it's possible, but with the Master controller it's impossible
The manual about Profibus for Advant is quite good, use it!
It's not the easiest task, but it can be done if you have a good understanding of how Profibus works. There are no modern tools that can help you, so you need to understand every bit and byte.
by MyMe "
by MyMe Rank: 13420 on 9/3/2016 7:08:28 AM | Like (0) | Report
Which gs-file are you using?
by Stefan Stromqvist
Sorry, fieldbuses is not my area.
Add new comment