Smart Client error
I am installing Smart client 2.2 rev c. Trying to in install server on windows 2012.
Please see error attached.
Answers
Hello,
did you check all prerequisites before start the installation?
It looks like you haver a problem with .net application.
Regards
The CD is labelled "MYCD" in the attached image.
--> is it a home made CD? Is it known to be okay??
The error code translates to 0x80040707
(hint type the large decimal negative value into calc.exe then swap to hexadecimal presentation).
Searching internet for "cocreateobjectdotnet 80040707" return a number of suggestions. Plain guessing from the few articles I read:
1. Try "Run as" (administrator and with no protection)
2. Try copying files from CD over to hard disk and install from there.
But I guess if a person better skilled in Smart Client than myself sees this he/she can probably easily tell if its a known problem of some kind and provide a workaround.
Hi Yagishen.
Do you have solved the Problem?
I have the same error.
Add new comment