CI861 is hot swappable?
HI,
Is CI 861 (VIP) card is hot swappable? or I need to power down the controller to replace the cards?
Thanks.
Voted best answer
look in http://www402.abbext.com/Technical-document-CI861-CI864-q2248819.aspx
3.6 Known Software and documentation problems
"Hot removal of the CI861 does not work in SV5.1 systems. Removal of the CI861
module may crash the controller when communication is active"
Add new comment