Using Actual5 parameter in ACS 800 Drive and RETA02 Module
Hello all,
I have an application where I need to use the Actual5 Parameter from an ACS800 drive configured to provide a torque value. I'm using a RETA-02 module and PP04 interface to the ACS800. The application uses the PCDevLib MotorVarSpeedBus object.
My question is how to configure the drive to provide the actual5 value and what is the value the I would expect to see for a torque reading.
Thanks all in advance.
Answers
First of all read the user manual for RETA-02 (direct link below).
In manual you could find information how to configure a drive and how to read actual signals (in your case par. 01.05 TORQUE).
Add new comment