Hi govind,procedure for upgrading control builder3.2 to 5.1 version.
Presently we have control bulder 3.2 version which is running on window 2000 plateform.
We would like to upgrade to 5.1 version which support windows 7 plateform.
Thanks to provide procedure for upgrading with latest version.
Answers
Hello,
I did that for Compact Control Builder.
As I remember, you need to go from 3.2 to 4.1 and then from 4.1 to 5.1.
You can write in Help - Index in CBM 5.1 "upgrade project" to see that. Some comments from help:
- Select Tools > Maintenance > Upgrade Project.
- From the Open Project dialog, select the project to be upgraded and click Open.
- From the Save Upgraded Project As dialog, click Save
It is only possible to upgrade control builder projects that are on file format like compact control builder. It is only possible to upgrade compact control builder projects from system version 4.1 and later.
A Compact Control Builder 5.0.2 project containing CI851 or CI852 modules must not be upgraded to BasicHwLib 5.1-0, but shall be kept with BasicHwLib 5.0-2.
Add new comment