HW Connection Error
Form time to time when I download the application to the controler there is the following Error and I need to proceed a coldstart.
Error 9166: Controller:HW Connection : The I/O-connections for Application XXXX are not possible to analyze. Cold restart of the application is required
Does anybody can help me with this Error
Answers
Pls attach the controller log and also specify the system version using.
Source:
Are you using a BPCS or a SIS controller? It can be analyzed better if you provide the controller logs
Add new comment