"End Node" parameter in CI855
I am about to configure a new AC800M with, amongst others, a CI855 card. The configuration editor for CI855 has a parameter called "End Node".
The help topics does not provide much details on the parameter, and I was wondering if anyone could explain briefly the consequence of setting the parameter to false/true respectively.
The default value is "false". However, we have an old CI855 where the parameter is set to "true".
Thanks.
Voted best answer
End Node = true means that all routing messages are disabled. Unless you're having load issues, don´t bother!
Add new comment