800xA for Advant Master : faceplate is not working after MB300 uploading
Hello,
I wanted to add new tags to the system. 800xA 5.1 FP4 advant master.
After creating PIDCONA with CRDB command on Online builder,
and connecting PC program, I did MB300 Uploader.
Uploading process is completed well. But, the tag is not working. I couldn't operate the tag and no live data. I could check out data communiction on ONB but, not 800xA system.
Refer to the attached file. It shows you the faceplate is not working.
I created new DB and uploaded many time. I still have same result . New faceplate is not working. What happens to the system?
Your comment is really appreciated. Thanks in advance.
Answers
Data quality seem OK in faceplate (no red crosses). You can double check quality in Control Connection aspect (enable Subscribe for live data).
Likely, you have an issue with the PIDCONA configuration in the controller.
Compare this new inoperable with another working instance.
Are you absolutely sure that you didnt upload from FCB instead of the controller ( not likely, but just in case ;) )
In the control connection aspect for the new elements, check that the uploader has correctly set the LF (logical file) and LR (logical record) numbers for the new database elements. When you MDB a database element the LF and LR are shown at the top of the display. You can also MDB lf.lr which should show you the correct DB element.
You can actually completely shortcut the MB300 uploader by manualy creating objects in the Control Structure and setting the LF and LR values. However, I do NOT recommend you do this unless you know what youre doing.
Add new comment