Ac500-Eco Ftp doesn't work properly
I'm using automation builder 1.2.1 and I have added a FTP protocol to my device.
I have updated my device after a clean and rebuildall and login/run. THere are no anwers when i try to see the folders in my PLC with the command in internet explorer or chrome ftp://userdisk:user@100.43.1.232:21 where user is the password of userdisk area.
The same command in a windows folder works but I can see only the folder Webvisu, if I go into Vebvisu folder it crash... Any suggestion?
Have I to clean the plc with a fatory reset?
Voted best answer
Hi,
I do not use Ftp.
I encourted some problems chrome or ie with web server. Problem is related to java script was broken explorer side.
BR
Answers
The problem was the Web server not enabled in the configuration.
Problem seems PLC side. You can try different plc.
by FabioPD Rank: 285 on 8/9/2016 2:48:05 AM | Like (0) | Report
Sorry, in a windows folder works fine.
Add new comment