CI867 Slave redundancy
Can we have two CI867 as configured as single card , with different IP address .
Both acting as Modbus slave.
As per ABB Controller configuration, all modbus slave data's are mapped in Access variable.,Is it possible for this configuration to work.
Can AC800M Controller can act as two modbus TCP slave?
Answers
Hi,
In our project we have configured CI867 as redundant slave by giving offset IP 0.0.0.1
Its working fine.
If your question is regarding 2 different CI cards which are not redundant
I think only one card can handle all your access variables
Best Regards,
Add new comment