AC500 UDP Communications monitoring (ETH_UDP_INFO) not working
UDP Communication through ETH_UDP_STD_REC is working okay. I can see data from a UDP client okay.
But ETH_UDP_INFO function block doesnt show any diagnostic data. The EN and SLOT input pins are configured the same as ETH_UDP_STD_REC. The DONE output pin is TRUE and ERR is FALSE. All the other output pins are static at zero.
Can anybody explain if I should see a rolling figure for NUMR_BC output pin?
Answers
This question has not yet been answered.
Add new comment