Replication error bettreplication error between harmony connectivity servers
Do you know why I cannot do a replication between harmony connectivity servers?
Answers
The databases are synchronized as evidenced by the same sequence number. There are also no Online Changes. There is no need to replicate. Thus the button to replicate now is disabled.
No, the replication is not workinkg, i create a new tag, but it only apears on the primary Harmony server (HCS Prim)
It does appear the Red. HC has not replicated since July 27. Adding a New Tag should allow you to Replicate NOW. How did you add a new tag did you Import or add in Control Structure ? If I recall replication should occur at 4:00am Daily Regardless. You could backup the Red. ConfigServer Database and then Delete it and reboot it should replicate as it is The Subscriber.
Add new comment