PCC Viewer error
Hi everyone!
I have a problem when i try to open a minerals pcc viewer aspect on one object in particular.
It sends me an error "Run-time error "76" Path not found.
Its only in this particulas instance, the other isntances of the same object type are ok.
If i open the PCC viewer from an egineering workplace or conectivity server, the PCC viewer looks good.
Any ideas?
Answers
I'm not sure i understood correctly the PCC Viewer does not work on one object on some stations only? In this case it is most probably an installation issue, the installed Minerals Library Version differs between the stations.
Is this aspect overridden on this particular object (inherited = false)? This would most probably be an error and you can just delete the override.
Does the object have a unique name in the system? I think this is a requirement for the Aspect to work.
The name is unique, and i had the library.
I installed and uninstalled the CBM.
Thanks.
Add new comment