SIL fb in NON-SIL app
Hi,
I have instantiated a SIL function block in a NON-SIL application (AC800M v5.1 rev. D). The problem is in it's graphic item which has one button to be clicked. So, when I instantiate this graphic aspect on the graphic, first time the button can be clicked. But when I want to click it again, the button can't be clicked (its frame isn't risen when I put the mouse above it). So then I have to instantiate it again and then I can click it. The button can also always be clicked when I reach to it from Plant explorer (graphic aspect in control structure), but this is not a solution. I use this function block type also in other SIS controllers and SIL applications and it works fine. To resolve the problem, I was thinking to copy this fb type from SIS to BPCS library that I have created, remove the SIL-1/2 mark and instantiate it again in the NON-SIL application.
Does anybody knows a more elegant solution?
Tnx in advance,
Hrvoje
Answers
Why do you think the problem is related to SIL? This seems very unlikely.
You say you've tried deleting the FB from your code. Did you also delete the Button from your graphic and carefully check it's connections?
Add new comment