Is Panel Builder 800 5.1 compatible with 800xA version 6.0 ?
Hello Stefan,
Can you give me your comments about this question:
http://www402.abbext.com/Panel-Builde...
We have currently installed 800xA v. 6.0.0 and Panel Builder 800 5.1 installed in the same machine of the AS/CS (with Windows Server 2012) or in another machine (with Windows 7) like I explain in the question's description, the software can't connect through MMS and find the controller configuration in Control Builder M to acquire the name list.
Thank you in advance for your comments.
Voted best answer
Sorry, not my cup of tea
I'm rather sure that reading Access Variables over MMS is the same as in previous versions. Ie manual configuration (IP address + variable name) should work regardless of version of server and client. But, again this is not an area of my expertise.
Answers
From Control Builder you can use copy of variables / access variables and then paste them in Excel. Save as txt file with semi-comma separator.
For Panel Builder you can use import function.
This should work.
Panel Builder use the openinterface in Control Builder, so both Panel Builder and Control Builder need to be in same PC, then panel Builder can import the access variables from Control Builder to the Namelist in Panel Builder.
Note! Panel Builder 5.1 require 32-bit version in other case you have problem to type in alarms.
Add new comment