Change MB300 Network Number in 800xA V6.0.1
By mistake (wrong dokumantation) I have deployed the Advant CS pair with the wrong MB300 Net (11/12 instead of 15/0). The SCC don't let me change these values, so I change them in the system. But the MB300 Net don't let me edit the Network:
How could I do that or could I ignore that?
Thank you in advance!
Answers
Hi!
I have not tried this myself, but I think that you have to change the network number in "RTA Board Control" aspect on the "RTA Board" object.
In the end I build a new MB300 Network Object, in this case the aspect MB300 Net is set correct. Seems to me the only way.
Add new comment