There is a way to export a CBM project to compact without loosing cold retail values?
The CBM is a 5.0.2/2 and the migration is to a compact 5.0.2/5
everything seems fine using the tool of export in compact format and importing it but
there are some cold retain values (analog scaling parameters) that we can't find a way
to move from CBM to compact.
thanks in advance
Alessandro
Voted best answer
Please follow the following steps
1)Open the project in CBM
2)Go to online mode
3)From Control Builder menu bar, select Tools > Save ColdRetain Values.
4)Go offline and take the project backup.
5)From the OPC Server Configuration window, select File > Save Configuration.
The OPC configurations are saved in:
...\ABB Industrial IT Data\Control IT Data\OPC Server for
AC 800M\Files.
6)Copy the following OPC Server files from the OPC Server to a safe media:
• systemsetup.sys, located in:
...\ABB Industrial IT Data\Control IT Data\
OPC Server for AC 800M
• Configuration files (*.cfg), located in:
...\ABB Industrial IT Data\Control IT Data\
OPC Server for AC 800M\Files
Now for restore in the 5.0.2/5 system
Copy the following OPC Server files from the OPC Server to a safe media:
OPC Server for AC 800M
1. Restore the previously saved systemsetup.sys file to the following location:
ABB Industrial IT Data\Control IT Data\OPC Server for
AC 800M
2. Restore the configuration files (*.cfg) to the Files folder in the same location.
From the CCV selct tools--maintanance--restore--select complete restore and restore the project from
the safe media to a new folder in the following destination:
...\ABB Industrial IT Data\Engineer IT Data\
Compact Control Builder AC 800M\Projects
Add new comment