no connection whit OPC sever (OPCServer 6002 Failed to subscribe on 172.16.84.152)
Hi
I have problem to connect CPU AC800 PM891 whit OPC server AE
no problem whit OPC Data.
settings are ok was ranning well up to a certain date.
I attach files log
Answers
"Max Number of AE Subscribers" setting on CPU (0) at default value (1) and you have redundant OPC servers (or a Panel 800 subscribing as well)?
Increase, download and try connecting again!
Sometimes, in the past, stale/obsolete subscriptions could be left in CPU. If this happen, CPU must be reset, or an even larger "Max no..." must be downloaded. Search for bulletins describing this problem.
Add new comment