BMI - DOC Button single pulse
System 800xA 5.1 SP3
BMI 1.5-15
Screens in PG2
We are using the DOC button configured as single pulse, but the button "some times" freeze the command, and the variable ".value" still in "1" unless someone go to Control Builder and force to "0".
We check and didn't found any write command in the variable at Control Builder, so we don't have two different ways to send this command.
**We did a logic to mantain DOC block always in manual mode to be able to use the single pulse directly.
Any one has any similar case with problems when use DOC button as single pulse?
Thanks,
Best Regards,
Cinthia
Answers
This question has not yet been answered.
Add new comment