Download errors on Unit PPP settings come up.
Dear colleauges, thank you for help.
During the programm download in Control Builder it gives 4 errors:
1. Parameter "IP Adress" on unit "PPP" has an illegal value.
2. Parameter "Remote IP Adress" on unit "PPP" has an illegal value.
3. Parameter "Node Number" on unit "PPP" has an illegal value.
4. Parameter "Network Area" on unit "PPP" has an illegal value.
I did screenshot on healthy download two month ago, and compared it with current settings in PPP Unit, it is the same. Can you please advise what could be the reason of these errors and how can I fix it?
Answers

Here is the screenshot!
Hi
I got the same error in my system when i changed th ipaddress to some illegal value under AC800M ---> 4 Com ---> PPP settings.
I guess you might have changed the default value, pls revertback it to theoriginal values.
Below is the standard settings you will get when you create new controller.
I hope this solvesyour problem.
Regards
Poorna
Add new comment