Controller Crash on Warm Download
Dear Stephan,
I was hoping if you could provide some urgent support. I am on site before startup phase and everything was seeming to be wokring fine in our system. However, I made a warm download after making some minor changes in my application and controller along with its redundant controller went in fault. It is worth noting that it downloaded perfectly when I downloded in an empty controller, but the issue only forward on a warm download. Most of the testing was done on a simulator where no such issue was ever seen. I am using 800xA, 5.1 FP4 and this is the HI controller PM865 with SM811. I have attaced the controller logs (2 warm downloads in quick succession) for your reference. I would be highly grateful if anyone else has anything to add on this?
Regards,
Haidar
Answers
Sorry, AC 800M, especially safety is not my cup of tea. I'm on vacation with few fellow colleagues to ask.
I can see "Out of memory" in the SM log, but if that is relevant or not I have no idea of.
As usual, for professional support, have a support case submitted with your regional ABB support center.
Dear colleague,
What was the applicaiton change that you made?.Was it related to communication/IAC variables?
by admin Rank: 46 on 7/17/2016 7:02:27 PM | Like (0) | Report
Strongly suggested to get connect with local ABB support people for this type of cases, that will be proper channel to get support incase of crisis and running plant cases...
Thanks for your understanding.
-/Admin
Add new comment