800xA 6.0.1 Installation along with Melody Connect
Hello,
I have installed Melody S+ Melody using 2VAA006878_A_en_S__Engineering_for_Melody_1.1_SP1_DVD setup. And same was installed succesfully and could able to create new Projects etc.
And as a second step started with installing 800xA 6.0.1 on same node by selectign the Melody Connect.
But while deploying the System,the base system deploy is not completing and showing error as "Base System - Alarm Manager Service Firewall Configuration" .
Can anybody say how to remove this error and complete the Deploy of System.
Thanks in Advance!..
Answers
Can you attach the log file available in C:\Program Data\ABB\800xA\System Installer\Logs
Add new comment